Driving uptime through data – SKF at the 16th VDI conference
SKF will present developments in wind turbine bearing systems at the 16th VDI conference on slide and rolling bearings, held on 3-4 June 2025 in Schweinfurt, Germany. Topics include sensorized rolling elements and validation testing, with a guided tour of SKF’s Sven Wingquist Test Center also available.
Strengthening the spin – SKF course in bearing solutions for wind turbines
SKF has recently concluded its highly anticipated three-day training on wind turbine bearing technologies in Schweinfurt, Germany. The event brought together a select group of 15 professionals from diverse engineering fields for an in-depth exploration of SKF’s wind turbine bearing solutions.
The Sven Wingquist Test Center – Chartering the future of wind power generation
Nestled on the outskirts of Schweinfurt, Germany, the Sven Wingquist Test Center – the winner of an International Architecture Award 2018 – is a sight to behold. But what distinguishes it in terms of its contributions to the wind industry?
Strong and robust – Putting tailored heat-treated gearbox bearings to the test
Robust bearings are the key to a long-lasting wind turbine. To evaluate their surface and subsurface robustness and minimize failures, SKF has further developed the SKF Generalized Bearing Life Model (GBLM). During the "Bearing World by FVA" conference, the company presented its application of the SKF DuraPro for wind turbine gearboxes.
Towards Testing 4.0 – How SKF helps shape the future of wind energy
The demand on wind turbines is increasing. It is the same for the roller bearings that enable their smooth operation. These bearings must withstand ever-higher loads, moments, and harsh conditions, while still increasing efficiency and reliability as demand rises. To help companies meet these challenges, SKF analyzes large-scale roller bearing behavior under extreme and real conditions at the Sven Wingquist Test Center.
Supply chain transparency – Introducing a new solution for streamlining O&M
With the wind energy industry facing increased competition and decreasing margins, SKF and Boralex have teamed up. Their joint project, called the Wind Turbine Reliability Dashboard, will help predict maintenance requirements and streamline supply chain management, lowering overall operating costs and increasing profitability in the process.
Taking the environmental LEED – SKF test center rewarded for eco-friendliness
Leadership in Energy and Environmental Design (LEED) is a global green building certification system. Since 2010, SKF decided to construct all new buildings in compliance with LEED. It has kept its word and was recognized with the gold certification status for the Sven Wingquist Test Center in Schweinfurt, Germany.
A visual representation – Digitally demonstrating wind turbine components
A company develops a new wind turbine component; but without a platform to showcase this, it may be difficult to convince interested parties of its advantages. So how can manufacturers display key turbine parts, many of which are massive or only functional within a working turbine, to an audience? The digital era may present yet another solution.
Testing reaches new heights – SKF test center is setting new industry standards
In July 2017, the Sven Wingquist Test Center was opened in Schweinfurt, Germany. The aim of this project was to improve current testing software and standards and to develop more reliable large-size bearings. The facility is up and running and providing the wind power industry with a unique service.