Weathering the next storm – Offshore turbines face rising wind extremes
Wind drives offshore turbines, but it can also destroy them. As storms grow stronger and less predictable, the safety margins once built into turbine designs are under pressure. The question is no longer whether turbines can harness the wind, but whether they can survive it.
Gone with the wind – The phaseout of SF6
In April, the European Council made its first overture to phase out SF6 and other F-gas-based technology in current wind farm installations. The greenhouse gas accounts for a staggering portion of our current climate emergency, outshining even carbon dioxide. Though SF6’s hitherto entrenched role in big wind may present challenges in navigating the rollback, the change will ultimately be worth it for a more sustainable future.
Port of call – Navigating the future of offshore wind farming
The role of ports in offshore wind farming cannot be underestimated. As we transition from the use of hydrocarbons to renewable energy, the wind industry seeks to maximize optimization of portside facilities. It will achieve this by continuing to identify favorable portside locations and lobbying for change at TENT-T.
5 ways to transform the world – Building a sustainable energy future with wind
The urgent need to transition to renewable energy sources has never been clearer. Sustainable technologies are already cost-effective but making them the world's main energy source requires additional action. In this article, we look at five changes that are inevitable to achieve a cleaner, greener future.
Mining – How the industry is getting greener with wind
The mining industry is not exactly considered a pioneer when it comes to sustainability. But the industry is also key to the energy transition – after all, green technology relies heavily on certain metals and other materials. Wind energy could solve the dilemma.
Missing the 1.5°C target? – Highlights of COP27
Limiting global warming to a maximum of 1.5° C compared to preindustrial levels has become prevalent on the agenda of many countries. It was also part of the agenda at the 27th annual UN Climate Change Conference, which recently took place in Egypt. What did the decision makers discuss?
No need to choose – Preserving species and fighting climate change
Wind energy is a driving force of the energy transition. Especially offshore wind parks have proven to be extremely promising due to their ability to produce massive amounts of energy. Yet, marine biologists are concerned about the influence the construction may have on the underwater environment. Does this mean we have to sacrifice climate protection for the sake of marine flora and fauna?
On the edge – What saving the planet means for the wind industry
The 2022 report of the Intergovernmental Panel on Climate Change (IPCC) has brought the importance of climate protection back to the forefront worldwide. Let us take a look at the global wind energy market: What changes can operators expect in the coming years?
NEOM: The future’s new home? – All about the Red Sea’s green city
In renewable energy’s relatively short existence, no project as ambitious as NEOM has ever been dreamed of. But Saudi Arabia’s potentially greener-than-green city is now under construction. Compared with the erection of the pyramids, but ready in ten years, NEOM and THE LINE represent a massive mindset shift in the region.