Don’t miss anything!

Subscribe to our newsletter to stay up to date on the wind energy industry.

Sign Up

Furious seas, steady solutions – Predictive maintenance for North Sea wind turbines

The North Sea is home to numerous wind turbines which face unique challenges due to the hostile environment. However, with the advent of advanced diagnostic tools like the SKF Multilog IMx machine monitoring devices, the maintenance and efficiency of these wind turbines have seen significant improvements.

The North Sea, with its strong and consistent winds generated by temperature differences between land and sea, offers ideal conditions for wind-powered electricity generation. Additionally, the region’s relatively shallow waters facilitate the anchoring of wind turbine foundations, enhancing cost-effectiveness in construction. However, these same winds can lead to rough seas, complicating access for repairs and routine maintenance of the turbines, thereby adding to the complexity and cost of upkeep.

In such demanding environments, the SKF Multilog IMx machine systems, IMx-8 and IMx-16, are a wise choice. These systems continually track various parameters such as vibration, temperature, and rotational speed, which are crucial for the early detection of potential issues like bearing faults, gear problems, or misalignment in wind turbines.

Remote data access and predictive maintenance

The SKF Multilog IMX systems provide a significant advantage with their capability to remotely transmit data. This allows operators to assess the health and performance of each turbine from a distance, eliminating the need for frequent on-site visits.

Strong winds, high humidity, and exposure to saltwater in the North Sea can lead to corrosion and increased wear and tear on turbine components. Using data provided by the SKF Multilog IMX systems, operators can transition to predictive maintenance. This approach involves performing maintenance based on the equipment’s condition rather than following a fixed schedule, offering a more efficient and cost-effective method. It reduces the risk of catastrophic failures, enhances safety, and ensures the reliable operation and longevity of the turbines.

Real-world success: C-Power offshore wind farm

The use of SKF Multilog IMX systems at the C-Power wind farm in the North Sea showcases their effectiveness in a real-world scenario. The systems collect crucial data, particularly from vibration sensors in generator bearings and gearboxes. The data is then analyzed at SKF’s Remote Diagnostics Services Centre, facilitating early problem detection.

For more information about the wind farm and the profound impact of SKF Multilog IMX systems in the North Sea, read the full story.

Don’t miss anything!

Subscribe to our newsletter to stay up to date on the wind energy industry.

Sign Up

Related articles

Technology

From deep blue to green – Advancements fueling offshore wind power

Operations
Testing the boundaries – Turbine bearings in extreme environments

Testing the boundaries – Turbine bearings in extreme environments

Technology
Let’s talk safety: What kind of maintenance do wind turbines need?

Let’s talk safety – What kind of maintenance do wind turbines need?