Don’t miss anything!

Subscribe to our newsletter to stay up to date on the wind energy industry.

Sign Up

Weathering the next storm – Offshore turbines face rising wind extremes

Wind drives offshore turbines, but it can also destroy them. As storms grow stronger and less predictable, the safety margins once built into turbine designs are under pressure. The question is no longer whether turbines can harness the wind, but whether they can survive it.

Offshore wind farms across Europe and Asia now face conditions that change faster than design standards can track. Research from the Southern University of Science and Technology in China shows that extreme winds are becoming more frequent, pushing turbines beyond their design limits.

A shrinking buffer between design and reality

According to the study, wind speeds are rising along more than 60 percent of the world’s coastlines. Nearly one in five coastal areas already experiences winds that exceed the threshold for Class III turbines. Each turbine class includes a safety margin to absorb rare gusts without damage: Class III turbines are built for winds up to 37.5 m/s, Class II for 42.5 m/s, and Class I for 50 m/s. The researchers found that as storms intensify, those margins are disappearing, increasing mechanical strain, especially in older turbines built on outdated climate data.

The study also highlights that some of the most exposed wind farms lie off south-east England, the German coast, Denmark, the Netherlands, Belgium, and Sweden. Even small increases in wind speed can sharply raise stress on key components.

At higher altitudes, the research shows that risks rise further. At 200 m hub height, more than half of offshore sites exceed the Class III limit, compared with one-third at 80 m. The chance of Class I-level extremes increases more than tenfold between 100 and 200 m, meaning newer, taller turbines face far greater exposure.

Warning signs from the field

In 2024, Typhoon Yagi damaged six turbines near Hainan, China, one of the worst weather-related failures on record. Extreme winds now cause more than half of all turbine breakdowns. Even when turbines remain operational, the added strain accelerates wear, shortens lifespans, and increases unplanned shutdowns.

Resilience will define the next generation of wind farms

The offshore wind industry is beginning to adapt, using longer climate records, stronger structures in high-risk zones, and updated project standards. Many developers are exploring higher design classes and upgrading components to meet evolving conditions.

Part of that progress comes from materials innovation. Bearings such as SKF’s DuraPro series, available for both wind turbine gearboxes and main shafts, are engineered to handle higher dynamic loads and maintain reliability under variable winds.

Such advances, combined with better forecasting and planning, will help offshore turbines remain efficient and resilient in the decades ahead.

Don’t miss anything!

Subscribe to our newsletter to stay up to date on the wind energy industry.

Sign Up

Related articles

Wind News
Tougher bearings for tougher conditions – SKF DuraPro for wind turbine main shafts

Tougher bearings for tougher conditions – SKF DuraPro for wind turbine main shafts

Wind News
Thunderbolts and lightning not very frightening – Tornadoes: a different story?

Thunderbolts and lightning not very frightening – Tornadoes: a different story?

Wind News

Big year ahead for Europe – Over 6 GW of offshore wind set to move forward