Tougher bearings for tougher conditions – SKF DuraPro for wind turbine main shafts
Out in the North Sea, a wind turbine keeps turning, no matter the wind, rain, or crashing waves. But inside, where no one sees, many components keep it running, and few are as critical as the main shaft bearing. If it wears down prematurely, performance declines, maintenance costs rise, and in the worst cases, unplanned downtime follows.
Mounting matters – Proper bearing installation keeps wind turbines spinning
Bearings in wind turbines support the rotating shafts and minimize friction between moving parts. Improper bearing mounting in wind turbines can lead to several serious consequences, affecting both the performance and lifespan of the turbine.
Full float ahead – First turbine assembled for Gulf of Lion wind farm
Assembly is picking up pace on France’s Mediterranean coast, where the first floating turbine of the EFGL pilot project has been completed at Port-La Nouvelle. The milestone marks the start of offshore deployment for one of Europe’s most closely watched wind technology trials.
The power of bubbles – Offshore wind construction goes quieter
Off the UK coast, a wall of rising bubbles is quietly making a big difference. For the first time in UK waters, a bubble curtain is being used during offshore wind farm construction. The technology is now in action at the Sofia offshore wind farm, one of Europe’s largest energy projects.
The power of lubrication – What every wind turbine operator should know
When it comes to any type of machinery, including wind turbines, proper lubrication is one of the simplest yet most important ways to keep everything running smoothly. Understanding how lubrication works can save a lot of time, money, and headaches. This article takes a closer look at oil and grease — what they are, how they work, and why they matter.
Driving uptime through data – SKF at the 16th VDI conference
SKF will present developments in wind turbine bearing systems at the 16th VDI conference on slide and rolling bearings, held on 3-4 June 2025 in Schweinfurt, Germany. Topics include sensorized rolling elements and validation testing, with a guided tour of SKF’s Sven Wingquist Test Center also available.
The future of wind energy – Turbine innovations from Enercon, Vestas, and Nordex
The Enercon E-175 EP5, Vestas V172-7.2 MW, and Nordex N175/6.X are turbines to watch in the coming years, each bringing innovations that enhance performance while cutting costs. Here’s a closer look at what makes them stand out.
Above and beyond – From the depths of coal mines to sky-high wind turbines
Germany is turning a former coal mine in Lusatia, in the state of Brandenburg, into a center for renewable energy with Gicon’s construction of what will soon be the world’s tallest onshore wind turbine.
Birds steer clear – Study in Norway finds zero collisions at floating wind farm
A two-year monitoring study at Norway’s Marine Energy Test Center has revealed that no bird collisions occurred with its TetraSpar floating offshore wind turbine. This milestone study sheds new light on the compatibility of floating wind turbines and bird populations, a concern for both renewable energy advocates and environmental groups.